USART Control and Status Register n A

Name:
UCSRA
Offset:
0xC0 + n*0x08 [n=0..1]
Reset:
0x20
Access:
-
Bit76543210
RXCnTXCnUDREnFEnDORnUPEnU2XnMPCMn
AccessRR/WRRRRR/WR/W
Reset00100000

Bit 7 – RXCn: USART Receive Complete

USART Receive Complete

This flag bit is set when there are unread data in the receive buffer and cleared when the receive buffer is empty (i.e., does not contain any unread data). If the receiver is disabled, the receive buffer will be flushed and consequently, the RXC bit will become zero. The RXC flag can be used to generate a receive complete interrupt (see the description of the RXCIE bit).

Bit 6 – TXCn: USART Transmit Complete

USART Transmit Complete

This flag bit is set when the entire frame in the transmit shift register has been shifted out and there are no new data currently present in the transmit buffer (UDRn). The TXC flag bit is automatically cleared when a transmit complete interrupt is executed, or it can be cleared by writing a one to its bit location. The TXC flag can generate a transmit complete interrupt (see the description of the TXCIE bit).

Bit 5 – UDREn: USART Data Register Empty

USART Data Register Empty

The UDRE flag indicates if the transmit buffer (UDRn) is ready to receive new data. If UDRE is one, the buffer is empty, and therefore ready to be written. The UDRE flag can generate a data register empty interrupt (see the description of the UDRIE bit). UDRE is set after a reset to indicate that the transmitter is ready.

Bit 4 – FEn: Frame Error

Frame Error

This bit is set if the next character in the receive buffer had a frame error when received. I.e., when the first stop bit of the next character in the receive buffer is zero. This bit is valid until the receive buffer (UDRn) is read. The FEn bit is zero when the stop bit of received data is one. Always set this bit to zero when writing to UCSRnA.

This bit is reserved in Master SPI Mode (MSPIM).

Bit 3 – DORn: Data OverRun

Data OverRun

This bit is set if a data overrun condition is detected. A data overrun occurs when the receive buffer is full (two characters), it is a new character waiting in the receive shift register, and a new start bit is detected. This bit is valid until the receive buffer (UDRn) is read. Always set this bit to zero when writing to UCSRnA.

This bit is reserved in MSPIM.

Bit 2 – UPEn: USART Parity Error

USART Parity Error

This bit is set if the next character in the receive buffer had a parity error when received and the parity checking was enabled at that point (UCSRnC.UPM1 = 1). This bit is valid until the receive buffer (UDRn) is read. Always set this bit to zero when writing to UCSRnA.

This bit is reserved in MSPIM.

Bit 1 – U2Xn: Double the USART Transmission Speed

Double the USART Transmission Speed

This bit only has effect for the asynchronous operation. Write this bit to zero when using synchronous operation.

Writing this bit to one will reduce the divisor of the baud rate divider from 16 to 8 effectively doubling the transfer rate for asynchronous communication.

This bit is reserved in MSPIM.

Bit 0 – MPCMn: Multi-processor Communication Mode

Multi-processor Communication Mode

This bit enables the Multi-processor Communication mode. When the MPCM bit is written to one, all the incoming frames received by the USART receiver n that do not contain address information will be ignored. The transmitter is unaffected by the MPCM setting. Refer to Multi-Processor Communication Mode for details.

This bit is reserved in MSPIM.