An n-bit single-ended ADC converts a
voltage linearly between GND and VREF in 2n steps (LSBs). The lowest code is read as 0, and the highest
code is read as 2n-1.
Several parameters describe the deviation from the ideal behavior:
Offset: The deviation of the first transition (0x000 to 0x001) compared to the ideal transition (at 0.5 LSB). Ideal value: 0 LSB.
Figure 1. Offset Error
Gain error: After adjusting for offset,
the gain error is found as the deviation of the last transition (0x3FE to 0x3FF)
compared to the ideal transition (at 1.5 LSB below maximum). Ideal value: 0 LSB.
Figure 2. Gain Error
Integral Non-linearity (INL): After
adjusting for offset and gain error, the INL is the maximum deviation of an actual
transition compared to an ideal transition for any code. Ideal value: 0 LSB.
Figure 3. Integral Non-Linearity (INL)
Differential Non-linearity (DNL): The
maximum deviation of the actual code width (the interval between two adjacent
transitions) from the ideal code width (1 LSB). Ideal value: 0 LSB.
Figure 4. Differential Non-Linearity
(DNL)
Quantization Error: Due to the
quantization of the input voltage into a finite number of codes, a range of input
voltages (1 LSB wide) will code to the same value. Always ±0.5 LSB.
Absolute accuracy: The maximum
deviation of an actual (unadjusted) transition compared to an ideal transition for any
code. This is the compound effect of offset, gain error, differential error,
non-linearity, and quantization error. Ideal value: ±0.5 LSB.