9.2.1 Nonvolatile Memory (NVM) Control Register
Note:
- A BOR event Reset will indirectly clear WR by forcing the FSM to terminate the operation underway. The WR bit cannot be set if the operation target address held in the NVMADRx register falls within an unimplemented address space.
- Reset occurs only on POR or BOR, but the actual initial state of P2ACTIV that is visible to the user will depend upon which panel is determined to be Active after the Reset exit.
- A BMX address error is likely due to a bad NVMSRCADR value. The same error will generate a bus error trap via the interrupt controller. This will aid the software in diagnosing the issue.
- WRERR bit will remain set if an attempt is made to execute
(WR=
1) a reservedPROGOPcommand. WR bit will not remain set. - “Word” is defined to be a 128-bit data value plus ECC (140 bits total). However, each word program command may consist of a sequence of fractional word programming operations.
- Reserved when in Single Boot mode
(DUAL_BOOTPRESENT=
0).
| Symbol | Description | Symbol | Description | Symbol | Description |
|---|---|---|---|---|---|
| R | Readable bit | HC | Cleared by Hardware | (Gray cell) | Unimplemented |
| W | Writable bit | HS | Set by Hardware | X | Bit is unknown at Reset |
| C | Write to clear | S | Software settable bit | x | Channel number |
| Name: | NVMCON |
| Offset: | 0x3000 |
| Bit | 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | |
| Access | |||||||||
| Reset |
| Bit | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | |
| WRRE | WREC[2:0] | ||||||||
| Access | R/HS/HC | R/HS/HC | R/HS/HC | R/HS/HC | |||||
| Reset | 0 | 0 | 0 | 0 | |||||
| Bit | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | |
| WR | WREN | WRERR | NVMPIDL | Reserved[1:0] | |||||
| Access | R/S/HC | R/W | R/C/HS | R/W | R/HC/HS | R/HC/HS | |||
| Reset | 0 | 0 | 0 | 0 | 0 | 0 | |||
| Bit | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 | |
| LOCK | DRBV | MVMOP[3:0] | |||||||
| Access | R/W | R/C/HS | R/W | R/W | R/W | R/W | |||
| Reset | 0 | 0 | 0 | 0 | 0 | 0 | |||
Bit 20 – WRRE Program/Erase Reset Event bit
| Value | Description |
|---|---|
1 | Warm Reset request during program/erase operation |
0 | No event reported Write 0 to clear, writing 1 has no effect |
Bits 18:16 – WREC[2:0] Program/Erase Error Code bit
| Value | Description |
|---|---|
101 | Row programming operation not completed due to warm Reset |
100 | System bus error during row program operation |
| 011 | Error reported by Flash panel control logic |
| 010 | Security access control violation |
| 001 | Invalid program/erase operation (PROGOP) |
| 000 |
No error Unused codes are reserved Read as ‘000’ if WRERR=0 |
Bit 15 – WR Write Control bit(1)
| Value | Description |
|---|---|
1 | Initiates a memory or fuse element program or erase operation |
0 | Program or erase operation is complete and inactive |
Bit 14 – WREN Program/Erase Enable bit
| Value | Description |
|---|---|
1 | Allows program/erase cycles |
0 | Inhibits programming/erasing of memory or fuse elements; This bit cannot be updated if either the LOCK bit is set or the WR bit is set |
Bit 13 – WRERR Sequence Error Flag bit
| Value | Description |
|---|---|
1 |
Indicates an improper program or erase termination due to:
This bit cannot be set by software |
0 | Either a POR or BOR has occurred or software cleared the WRERR bit |
Bit 12 – NVMPIDL NVM Power Down in Idle Enable bit
| Value | Description |
|---|---|
1 | Flash panels enter a Sleep mode (very Low-Power mode) when device enters Idle mode |
0 | Keep Flash and fuse panels powered in Standby mode when device enters Idle mode |
Bits 11:10 – Reserved[1:0]
Bit 7 – LOCK Lock bit
| Value | Description |
|---|---|
1 | Program/erase functions are disabled until after the next Reset |
0 |
Program/erase functions are not disabled Write 1 to set, writing 0 has no effect |
Bit 6 – DRBV Data Read Buffer Valid bit
| Value | Description |
|---|---|
1 | Data read buffer holds valid data |
0 |
Data read buffer invalid Write 0 to clear, writing 1 has no effect |
Bits 3:0 – MVMOP[3:0] NVM Operation Select bits(4,5,6)
| Value | Description |
|---|---|
0111-0100 | Reserved |
0011 | The next WR command will perform a memory page erase operation |
0010 | The next WR command will perform a row program 1 operation |
0001 | The next WR command will perform a word program 1, 3 operation (data source: NVMDATAx) |
0000 | Reserved |