5.34.128.1 Arguments

-type power_scenario

Specifies the type of report to generate is a scenario power report.

-powerunit {value}

Specifies the unit in which power is set. The following table shows the acceptable values for this argument:

Value

Description

W

The power unit is set to watts

mW

The power unit is set to milliwatts

uW

The power unit is set to microwatts

-frequnit {value}

Specifies the unit in which frequency is set. The following table shows the acceptable values for this argument:

Value

Description

Hz

The frequency unit is set to hertz

kHz

The frequency unit is set to kilohertz

MHz

The frequency unit is set to megahertz

-toggle {value}

Specifies the toggle. The following table shows the acceptable values for this argument:

Value

Description

true

The toggle is set to true

false

The toggle is set to false

-scenario{value}

Specifies a scenario that the report is generated from.

-style {value}

Specifies the format in which the report will be exported. The following table shows the acceptable values for this argument:

Value

Description

Text

The report will be exported as Text file

CSV

The report will be exported as CSV file

-battery_life {value}

Specifies whether to include the battery life summary in the report. The following table shows the acceptable values for this argument:

Value

Description

true

Includes the battery life summary in the report

false

Does not include the battery life summary in the report

-battery_capacity {value}

Specifies the battery capacity in A*H.

-rail_breakdown {value}

Specifies whether to include the breakdown by rail summary in the report. The following table shows the acceptable values for this argument:

Value

Description

true

Includes the breakdown by rail summary in the report

false

Does not include the breakdown by rail summary in the report. This is the default value.

-type_breakdown {value}

Specifies whether to include the breakdown by type summary in the report. The following table shows the acceptable values for this argument:

Value

Description

true

Includes the breakdown by type summary in the report

false

Does not include the breakdown by type summary in the report. This is the default value.

-mode_breakdown {value}

Specifies whether to include a breakdown by mode in the report. The following table shows the acceptable values for this argument:

Value

Description

true

Includes the breakdown by mode in the report

false

Does not include the breakdown by mode in the report. This is the default value.

-opcond_summary {value}

Specifies whether to include the operating conditions summary in the report. The following table shows the acceptable values for this argument:

Value

Description

true

Includes the operating conditions summary in the report

false

Does not include the operating conditions summary in the report

{filename.rpt}

Specifies the name of the report.