21.7.3.6 Specific Input Constraints

Figure 21-22. Constraint Wizard – Specific Input Constraints
þÿ

In this window you can set constraints for specific input pins. You can modify the constraints from the grid.

To set a constraint for an input pin:
  1. Set the maximum and/or minimum input delay for selected pin in the grid.
  2. Click Next to go to the next step or Finish to exit the wizard.
Note: This option is available only when there is an input pin in your design.

Double-click the Port Name or Clock header in the table to change the sorting order by input port name or clock name.