5.34.118.3 Arguments
-placer_high_effort value
The following table shows the acceptable values for this argument:
Value | Description |
off | Disables physical synthesis of combinational logic. This is the default. |
on | Enables physical synthesis of combinational logic |
-seq_opt value
The following table shows the acceptable values for this argument:
Value | Description |
off | Disables physical synthesis of sequential logic. This is the default. |
on | Enables physical synthesis of sequential logic in high-effort mode |
-mindel_repair value
The following table shows the acceptable values for this argument:
Value | Description |
off | Does not run minimum delay violations repair. This is the default. |
on | Enables repair of minimum delay violations during route |
-placer_seed value
An integer value that you can set to change the initial random seed number for the placement.
-show_placer_seed value
Causes Layout to display the initial random seed number used for the placement.