1.2.7.4.33 SYS_FS_FileDirectoryRemove Function
C
SYS_FS_RESULT SYS_FS_FileDirectoryRemove
(
const char* path
);Summary
Removes a file or directory.
Description
This function removes a file or directory as specified by the path.
Precondition
- The disk has to be mounted before a directory could be removed.
- The file or directory to be removed has to present.
- The file/sub-directory must not have read-only attribute (AM_RDO), or the function will be rejected with FR_DENIED.
- The sub-directory must be empty and must not be current directory, or the function will be rejected with FR_DENIED.
- The file/sub-directory must not be opened.
Parameters
| Param | Description |
|---|---|
| path | Path of the File or directory to be removed. |
Returns
SYS_FS_RES_SUCCESS - Indicates that the file or directory remove operation was successful.
SYS_FS_RES_FAILURE - Indicates that the file or directory remove operation was unsuccessful. The reason for the failure can be retrieved with SYS_FS_Error.
Example
SYS_FS_RESULT res;
res = SYS_FS_FileDirectoryRemove("Dir1");
if(res == SYS_FS_RES_FAILURE)
{
// Directory remove operation failed
}Remarks
None.