1.2.7.4.50 SYS_FS_FORMAT Macros
C
// The Values mentioned below should be aligned with values in ff.h #define SYS_FS_FORMAT_FAT 0x01 #define SYS_FS_FORMAT_FAT32 0x02 #define SYS_FS_FORMAT_EXFAT 0x04 #define SYS_FS_FORMAT_ANY 0x07 #define SYS_FS_FORMAT_SFD 0x08
Summary
Specifes the partitioning rule.
Description
This type specifies the partitioning rule.
When SYS_FS_FORMAT_FAT is specified, a primary partition occupying the entire disk space is created and then an FAT volume is created on the partition.
- It is usually used for hard disk, MMC, SDC, CFC and U Disk. It can divide a physical drive into one or more partitions with a partition table on the MBR. However Windows does not support multiple partition on the removable media.
When SYS_FS_FORMAT_SFD format is specified, the FAT volume starts from the first sector of the physical drive.
- It is non-partitioned method. The FAT volume starts from the first sector on the physical drive without partition table. It is usually used for floppy disk, micro drive, optical disk, and super-floppy media.
When SYS_FS_FORMAT_ANY format is specified FAT FS code decides on the format.