1.2.7.4.51 SYS_FS_FORMAT_PARAM Struct
C
typedef struct {
/* Specifies combination of FAT type flags, SYS_FS_FORMAT_XXX.
* These flags specify which FAT type to be created on the volume.
* If two or more types are specified, one out of them will be
* selected depends on the volume size and au_size.
* The default value is FM_ANY.
*/
uint8_t fmt;
/* Specifies number of FAT copies on the FAT/FAT32 volume.
* Valid value for this member is 1 or 2. If the FAT type is exFAT,
* this member has no effect.
*/
uint8_t n_fat;
/* Specifies alignment of the volume data area (file allocation pool,
* usually erase block boundary of flash media) in unit of sector.
* When a zero is given, alignment is decided on the block size.
*/
uint32_t align;
/* Specifies number of root directory entries on the FAT volume.
* Valid value for this member is up to 32768 and aligned to
* sector size / 32. If the FAT type is FAT32 or exFAT, this member
* has no effect.
*/
uint32_t n_root;
/* Specifies size of the allocation unit (cluster) in unit of byte.
* The valid value is power of 2 between sector size and
* 128 * sector size inclusive for FAT/FAT32 volume and up to 16 MB.
* When a zero is given, the cluster size depends on the volume size.
*/
uint32_t au_size;
} SYS_FS_FORMAT_PARAM;
Summary
SYS FS Drive Format parameter structure.
Description
Specifies the structure holding format options. This structure has to be filled and passed to SYS_FS_DriveFormat() API.
Remarks
None.