1.2.7.4.78 SYS_FS_MEDIA_BLOCK_EVENT Enum
C
typedef enum
{
/* Block operation has been completed successfully. */
SYS_FS_MEDIA_EVENT_BLOCK_COMMAND_COMPLETE = SYS_MEDIA_EVENT_BLOCK_COMMAND_COMPLETE,
/* There was an error during the block operation */
SYS_FS_MEDIA_EVENT_BLOCK_COMMAND_ERROR = SYS_MEDIA_EVENT_BLOCK_COMMAND_ERROR
} SYS_FS_MEDIA_BLOCK_EVENT;
Summary
Identifies the possible events that can result from a request.
Description
This enumeration identifies the possible events that can result from a media.
One of these values is passed in the "event" parameter of the event handling callback function that client registered with the driver by setting the event handler when a block request is completed.
Remarks
Refer to sys_media.h for actual enumerations.