1.2.7.4.1 SYS_FS_Initialize Function
C
SYS_FS_RESULT SYS_FS_Initialize
(
const void* initData
);Summary
Initializes the file system abstraction layer (sys_fs layer).
Description
This function initializes the abstraction layer (sys_fs layer) and sets up the necessary parameters.
Precondition
This is the first function to be called during usage of sys_fs. Calling other functions of sys_fs without initializing the sys_fs will cause unpredictable behavior.
Parameters
| Param | Description |
|---|---|
| initData | Pointer to an array of type SYS_FS_REGISTRATION_TABLE. The number of elements of array is decided by the definition SYS_FS_MAX_FILE_SYSTEM_TYPE. If the application uses one file system (say only FAT FS), SYS_FS_MAX_FILE_SYSTEM_TYPE is defined to be 1. Otherwise, if the application uses 2 file systems (say FAT FS and MPFS2), SYS_FS_MAX_FILE_SYSTEM_TYPE is defined to be 2. |
Returns
SYS_FS_RES_SUCCESS - SYS FS Layer was initialized successfully.
SYS_FS_RES_FAILURE - SYS FS Layer initialization failed. The reason for the failure can be retrieved with SYS_FS_Error.
Example
// This code shows an example of how the SYS FS is initialized // Only one file system is used #define SYS_FS_MAX_FILE_SYSTEM_TYPE 1 // Function pointer table for FAT FS const SYS_FS_FUNCTIONS FatFsFunctions = { .mount = FATFS_mount, .unmount = FATFS_unmount, .open = FATFS_open, .read = FATFS_read, .write = FATFS_write, .close = FATFS_close, .seek = FATFS_lseek, .tell = FATFS_tell, .eof = FATFS_eof, .size = FATFS_size, .fstat = FATFS_stat, }; const SYS_FS_REGISTRATION_TABLE sysFSInit [ SYS_FS_MAX_FILE_SYSTEM_TYPE ] = { { .nativeFileSystemType = FAT, .nativeFileSystemFunctions = &FatFsFunctions } }; SYS_FS_Initialize((const void *)sysFSInit);