1.2.7.4.30 SYS_FS_DirectoryMake Function
C
SYS_FS_RESULT SYS_FS_DirectoryMake
(
const char* path
);Summary
Creates a directory.
Description
This function creates a new directory as per the specified path.
Precondition
The disk has to be mounted before a directory could be made.
Parameters
| Param | Description |
|---|---|
| path | Path of the new directory |
Returns
SYS_FS_RES_SUCCESS - Indicates that the creation of the directory was successful.
SYS_FS_RES_FAILURE - Indicates that the creation of the directory was unsuccessful. The reason for the failure can be retrieved with SYS_FS_Error.
Example
SYS_FS_RESULT res;
res = SYS_FS_DirectoryMake("/mnt/mydrive/Dir1");
if(res == SYS_FS_RES_FAILURE)
{
// Directory make failed
}
Remarks
None.