1.2.7.4.32 SYS_FS_CurrentWorkingDirectoryGet Function
C
SYS_FS_RESULT SYS_FS_CurrentWorkingDirectoryGet
(
char *buff,
uint32_t len
);Summary
Gets the current working directory
Description
This function gets the current working directory path along with the working drive.
Precondition
At least one disk must be mounted.
Parameters
| Param | Description |
|---|---|
| buff | Pointer to a buffer which will contain the name of the current working directory and drive, once the function completes. |
| len | Size of the buffer. |
Returns
SYS_FS_RES_SUCCESS - Get current working directory operation was successful.
SYS_FS_RES_FAILURE - Get current working directory operation was unsucessful. The reason for the failure can be retrieved with SYS_FS_Error.
Example
SYS_FS_RESULT res; char buffer[16]; switch(appState) { case TRY_MOUNT: { if(SYS_FS_Mount("/dev/mmcblka1", "/mnt/myDrive", FAT, 0, NULL) != SYS_FS_RES_SUCCESS) { // Failure, try mounting again } else { // Mount was successful. Create a directory. appState = CREATE_DIR; } break; } case CREATE_DIR: { res = SYS_FS_DirectoryMake("Dir1"); if(res == SYS_FS_RES_FAILURE) { // Directory creation failed appState = ERROR; } else { // Directory creation was successful. Change to the new // directory. appState = CHANGE_DIR; } break; } case CHANGE_DIR: { res = SYS_FS_DirectoryChange("Dir1"); if(res == SYS_FS_RES_FAILURE) { // Directory change failed appState = ERROR; } else { // Directory change was successful. Get current working // directory appState = GET_CWD; } break; } case GET_CWD: { res = SYS_FS_CurrentWorkingDirectoryGet(buffer, 15); if(res == SYS_FS_RES_FAILURE) { // Get current directory operation failed appState = ERROR; } break; } }
Remarks
None.