1.2.7.4.40 SYS_FS_DriveLabelSet Function
C
SYS_FS_RESULT SYS_FS_DriveLabelSet
(
const char* drive,
const char *label
);Summary
Sets the drive label
Description
This function sets the label for the drive specified. If no drive is specified, the label for the current drive is set.
Precondition
At least one disk must be mounted.
Parameters
| Param | Description |
|---|---|
| drive | Pointer to string that holds the name of drive being for which the label is to be set. If this string is NULL, the label of the current drive is set by using this function. |
| label | Pointer to string which contains the label to be set. |
Returns
SYS_FS_RES_SUCCESS - Drive label set operation was successful.
SYS_FS_RES_FAILURE - Drive label set operation was unsucessful. The reason for the failure can be retrieved with SYS_FS_Error.
Example
SYS_FS_RESULT res;
switch(appState)
{
case TRY_MOUNT:
{
if(SYS_FS_Mount("/dev/mmcblka1", "/mnt/myDrive", FAT, 0, NULL) != SYS_FS_RES_SUCCESS)
{
// Failure, try mounting again
}
else
{
// Mount was successful. Get label now
appState = SET_LABEL;
}
break;
}
case SET_LABEL:
{
res = SYS_FS_DriveLabelSet("/mnt/myDrive", "MY_LABEL");
if(res == SYS_FS_RES_FAILURE)
{
// Drive label get failed
}
break;
}
}Remarks
None.