1.2.7.4.37 SYS_FS_CurrentDriveGet Function
C
SYS_FS_RESULT SYS_FS_CurrentDriveGet
(
char* buffer
);Summary
Gets the current drive
Description
This function gets the present drive being used. The drive information is populated in the buffer.
Precondition
The disk has to be mounted.
Parameters
| Param | Description |
|---|---|
| buffer | Pointer to buffer which will hold the name of present drive being used. |
Returns
SYS_FS_RES_SUCCESS - Current drive get operation was successful.
SYS_FS_RES_FAILURE - Current drive get operation was unsucessful. The reason for the failure can be retrieved with SYS_FS_Error.
Example
SYS_FS_RESULT res;
char buffer[255];
res = SYS_FS_CurrentDriveGet(buffer);
if(res == SYS_FS_RES_FAILURE)
{
// Operation failed.
}Remarks
None.