1.2.7.4.43 SYS_FS_DriveSectorGet Function
C
SYS_FS_RESULT SYS_FS_DriveSectorGet
(
const char* path,
uint32_t *totalSectors,
uint32_t *freeSectors
);Summary
Obtains total number of sectors and number of free sectors for the specified drive.
Description
Function to obtain the total number of sectors and number of free sectors in a drive (media).
Precondition
The drive for which the information is to be retrieved should be mounted.
Parameters
| Param | Description |
|---|---|
| path | Path to the volume with the volume name. The string of volume name must be preceded by "/mnt/". Also, the volume name and directory name must be separated by a slash "/". |
| totalSectors | Pointer to a variable passed to the function, which will contain the total number of sectors available in the drive (media). |
| freeSectors | Pointer to a variable passed to the function, which will contain the free number of sectors available in the drive (media). |
Returns
SYS_FS_RES_SUCCESS - Sector information get operation was successful.
SYS_FS_RES_FAILURE - Sector information get operation was unsucessful. The reason for the failure can be retrieved with SYS_FS_Error.
Example
uint32_t totalSectors, freeSectors; SYS_FS_RESULT res; if(SYS_FS_Mount("/dev/mmcblka1", "/mnt/myDrive", FAT, 0, NULL) != SYS_FS_RES_SUCCESS) { // Failure, try mounting again } else { // Mount was successful. // Do other FS stuffs. } // Perform usual FS tasks. //.... //.... // Now, determine the total sectors and free sectors res = SYS_FS_DriveSectorGet("/mnt/myDrive", &totalSectors, &freeSectors); if(res == SYS_FS_RES_FAILURE) { //Sector information get operation failed. }
Remarks
None.