1.2.7.4.31 SYS_FS_DirectoryChange Function
C
SYS_FS_RESULT SYS_FS_DirectoryChange
(
const char* path
);Summary
Changes to a the directory specified.
Description
This function changes the present directory to a new directory.
Precondition
The disk has to be mounted and the directory to be changed must exist.
Parameters
| Param | Description |
|---|---|
| path | Path of the directory to be changed to. |
Returns
SYS_FS_RES_SUCCESS - Indicates that the directory change operation was successful.
SYS_FS_RES_FAILURE - Indicates that the directory change operation was unsuccessful. The reason for the failure can be retrieved with SYS_FS_Error.
Example
SYS_FS_RESULT res;
res = SYS_FS_DirectoryChange("Dir1");
if(res == SYS_FS_RES_FAILURE)
{
// Directory change failed
}
Remarks
None.