1.2.7.4.6 SYS_FS_FileOpen Function
C
SYS_FS_HANDLE SYS_FS_FileOpen
(
const char* fname,
SYS_FS_FILE_OPEN_ATTRIBUTES attributes
);Summary
Opens a file.
Description
This function opens a file with the requested attributes.
Precondition
Prior to opening a file, the name of the volume on which the file resides should be known and the volume should be mounted.
Parameters
| Param | Description |
|---|---|
| fname | The name of the file to be opened along with the path. The fname format is as follows: "/mnt/volumeName/dirName/fileName". volumeName is the name of the volume/drive. dirName is the name of the directory under which the file is located. fileName is the name of the file to be opened. The "/mnt/volumeName" portion from the fName can be omitted if the SYS_FS_CurrentDriveSet () has been invoked to set the current drive/volume. |
| attributes | Access mode of the file, of type SYS_FS_FILE_OPEN_ATTRIBUTES |
Returns
On success - A valid file handle will be returned
On failure - SYS_FS_HANDLE_INVALID. The reason for the failure can be retrieved with SYS_FS_Error.
Example
SYS_FS_HANDLE fileHandle;
fileHandle = SYS_FS_FileOpen("/mnt/myDrive/FILE.txt", (SYS_FS_FILE_OPEN_READ));
if(fileHandle != SYS_FS_HANDLE_INVALID)
{
// File open succeeded.
}
else
{
// File open failed.
}// Using SYS_FS_CurrentDriveSet () function. SYS_FS_HANDLE fileHandle; SYS_FS_CurrentDriveSet("/mnt/myDrive"); fileHandle = SYS_FS_FileOpen("FILE.txt", (SYS_FS_FILE_OPEN_READ)); if(fileHandle != SYS_FS_HANDLE_INVALID) { // File open succeeded. } else { // File open failed. }
Remarks
None.