1.2.7.4.16 SYS_FS_FileError Function
C
SYS_FS_ERROR SYS_FS_FileError
(
SYS_FS_HANDLE handle
);Summary
Returns the file specific error.
Description
For file system functions which accepts valid handle, any error happening in those functions could be retrieved with SYS_FS_FileError. This function returns errors which are file specific.
Please note that if an invalid handle is passed to a file system function, in such a case, SYS_FS_FileError will not return the correct type of error, as the handle was invalid. Therefore, it would be prudent to check the errors using the SYS_FS_Error function.
Precondition
This function has to be called immediately after a failure is observed while doing a file operation. Any subsequent failure will overwrite the cause of previous failure.
Parameters
| Param | Description |
|---|---|
| handle | A valid file handle |
Returns
Error code of type SYS_FS_ERROR.
Example
... SYS_FS_HANDLE fileHandle; const char *buf = "Hello World"; size_t nbytes; size_t bytes_written; fileHandle = SYS_FS_FileOpen("/mnt/myDrive/FILE.txt", (SYS_FS_FILE_OPEN_WRITE)); if(fileHandle != SYS_FS_HANDLE_INVALID) { // File open is successful } // Write data to the file bytes_written = SYS_FS_FileWrite(fileHandle, (const void *)buf, nbytes); if(bytes_written == -1) { // error while writing file // find the type (reason) of error err = SYS_FS_FileError(fd); }
Remarks
None.