1.2.7.4.4 SYS_FS_Unmount Function
C
SYS_FS_RESULT SYS_FS_Unmount
(
const char *mountName
);Summary
Unmounts the disk/volume for the file system.
Description
This function removes (unmounts) the attachment of the volume from the file system.
Precondition
The volume name has to be know in order to pass as input to Unmount. The specified volume name to be unmounted should have been already mounted.
Parameters
| Param | Description |
|---|---|
| mountName | Mount name for the volume to be unmounted. The mount name has to be preceded by the string "/mnt/". |
Returns
SYS_FS_RES_SUCCESS - Unmount was successful.
SYS_FS_RES_FAILURE - Unmount was unsuccessful. The reason for the failure can be retrieved with SYS_FS_Error.
Example
if(SYS_FS_Unmount("/mnt/myDrive") != SYS_FS_RES_SUCCESS)
{
// Failure, try unmounting again
}
else
{
// Unmount was successful.
}