2.7.2.11 MemManage Fault Status Register

The flags in the MMFSR indicate the cause of memory access faults. The bit assignments are:

Figure 2-38. MMFSR Bit Assignments
Table 2-58. MMFSR Bit Assignments
BitsNameFunction
[7]MMARVALIDMemManage Fault Address Register (MMFAR) valid flag:

0: value in MMAR is not a valid fault address

1: MMAR holds a valid fault address.

If a MemManage fault occurs and is escalated to a HardFault because of priority, the HardFault handler must set this bit to 0. This prevents problems on return to a stacked active MemManage fault handler whose MMAR value has been overwritten.

[6:5]Reserved.
[4]MSTKERRMemManage fault on stacking for exception entry:

0: no stacking fault

1: stacking for an exception entry has caused one or more access violations.

When this bit is 1, the SP is still adjusted but the values in the context area on the stack might be incorrect. The processor has not written a fault address to the MMAR.

[3]MUNSTKERRMemManage fault on unstacking for a return from exception:

0: no unstacking fault

1: unstack for an exception return has caused one or more access violations.

This fault is chained to the handler. This means that when this bit is 1, the original return stack is still present. The processor has not adjusted the SP from the failing return, and has not performed a new save. The processor has not written a fault address to the MMAR.

[2]Reserved
[1]DACCVIOLData access violation flag:

0: no data access violation fault

1: the processor attempted a load or store at a location that does not permit the operation.

When this bit is 1, the PC value stacked for the exception return points to the faulting instruction. The processor has loaded the MMAR with the address of the attempted access.

[0]IACCVIOLInstruction access violation flag:

0: no instruction access violation fault

1: the processor attempted an instruction fetch from a location that does not permit execution.

This fault occurs on any access to an XN region, even when the MPU is disabled or not present.

When this bit is 1, the PC value stacked for the exception return points to the faulting instruction. The processor has not written a fault address to the MMAR.