7.4.1.1 HPDMA Empty Descriptor Register
| Bit Number | Name | Reset Value | Description |
|---|---|---|---|
| 0 | HPDMAEDR_DCP_EMPTY[0] | 1 | Descriptor 0 is empty and ready for software configuration. 1: Descriptor 0 is empty and ready to configure. 0: Descriptor 0 is already configured and descriptor transfer is in progress/queue. At the end of the descriptor transfer, either on transfer error or transfer done, the HPDMA controller asserts this bit High. |
| 1 | HPDMAEDR_DCP_EMPTY[1] | 1 | Descriptor 1 is empty and ready for software configuration. 1: Descriptor 1 is empty and ready to configure. 0: Descriptor 1 is already configured and descriptor transfer is in progress/queue. At the end of the descriptor transfer, either on transfer error or transfer done, the HPDMA controller asserts this bit High. |
| 2 | HPDMAEDR_DCP_EMPTY[2] | 1 | Descriptor 2 is empty and ready for software configuration. 1: Descriptor 2 is empty and ready to configure. 0: Descriptor 2 is already configured and descriptor transfer is in progress/queue. At the end of the descriptor transfer, either on transfer error or transfer done, the HPDMA controller asserts this bit High. |
| 3 | HPDMAEDR_DCP_EMPTY[3] | 1 | Descriptor 3 is empty and ready for software configuration. 1: Descriptor 3 is empty and ready to configure. 0: Descriptor 3 is already configured and descriptor transfer is in progress/queue. At the end of the descriptor transfer, either on transfer error or transfer done, the HPDMA controller asserts this bit High. |
| 4 | HPDMAEDR_DCP_CMPLET[0] | 0 | Descriptor 0 transfer complete. 1: Descriptor 0 transfer completed successfully. 0: Descriptor 0 transfer not completed. When the descriptor 0 transfer is completed, either with transfer error or transfer done, HPDMA controller asserts this bit High. This bit is cleared on writing ‘1’ to the HPDMAICR_CLR_XFR_INT[0] bit of the HPDMA Interrupt Clear register or when the HPDMACR_DCP_VALID[0] bit of descriptor 0 Control register is set. |
| 5 | HPDMAEDR_DCP_CMPLET[1] | 0 | Descriptor 1 transfer complete. 1: Descriptor 1 transfer completed successfully. 0: Descriptor 1 transfer not completed. When the descriptor 1 transfer is completed, either with transfer error or transfer done, the HPDMA controller asserts this bit High. This bit is cleared on writing ‘1’ to the HPDMAICR_CLR_XFR_INT[1] bit of the HPDMA Interrupt Clear register or when the HPDMACR_DCP_VALID[1] bit of the descriptor 1 Control register is set. |
| 6 | HPDMAEDR_DCP_CMPLET[2] | 0 | Descriptor 2 transfer complete. 1: Descriptor 2 transfer completed successfully 0: Descriptor 2 transfer not completed When the descriptor 2 transfer is completed, either with transfer error or transfer done, the HPDMA controller asserts this bit High. This bit is cleared on writing ‘1’ to the HPDMAICR_CLR_XFR_INT[2] bit of the HPDMA Interrupt Clear register or when the HPDMACR_DCP_VALID[2] bit of the descriptor 2 Control register is set. |
| 7 | HPDMAEDR_DCP_CMPLET[3] | 0 | Descriptor 3 transfer complete. 1: Descriptor 3 transfer completed successfully 0: Descriptor 3 transfer not completed When the descriptor 3 transfer is completed, either with transfer error or transfer done, the HPDMA controller asserts this bit High. This bit is cleared on writing ‘1’ to the HPDMAICR_CLR_XFR_INT[3] bit of the HPDMA Interrupt Clear Register or when the HPDMACR_DCP_VALID[3] bit of the descriptor 3 control register is set. |
| 8 | HPDMAEDR_DCP_ERR[0] | 0 | Descriptor 0 transfer error. 1: Descriptor 0 transfer error 0: No descriptor 0 transfer error This bit is asserted High if an error occurs during the descriptor 0 transfer at either source or destination end. This bit is cleared on writing ‘1’ to the HPDMAICR_CLR_XFR_INT[0] bit of the HPDMA Interrupt Clear register or when the HPDMACR_DCP_VALID[0] bit of the descriptor 0 control register is set. |
| 9 | HPDMAEDR_DCP_ERR[1] | 0 | Descriptor 1 transfer error. 1: Descriptor 1 transfer error 0: No descriptor 1 transfer error This bit is asserted High, if an error occurs during the descriptor 1 transfer at either source or destination end. This bit is cleared on writing ‘1’ to HPDMAICR_CLR_XFR_INT[1] of the HPDMA Interrupt Clear register, or when the HPDMACR_DCP_VALID[1] bit of Descriptor 1 control register is set. |
| 10 | HPDMAEDR_DCP_ERR[2] | 0 | Descriptor 2 transfer error. 1: Descriptor 2 transfer error 0: No descriptor 2 transfer error This bit is asserted High, if an error occurs during the descriptor 2 transfer at either source or destination end. This bit is cleared on writing ‘1’ to the HPDMAICR_CLR_XFR_INT[2] bit of the HPDMA Interrupt Clear register, or when the HPDMACR_DCP_VALID[2] bit of the descriptor 2 control register is set. |
| 11 | HPDMAEDR_DCP_ERR[3] | 0 | Descriptor 3 transfer error. 1: Descriptor 3 transfer error 0: No descriptor 3 transfer error This bit is asserted High, if an error occurs during the descriptor 3 transfer at either source or destination end. This bit is cleared on writing ‘1’ to HPDMAICR_CLR_XFR_INT[3] of the HPDMA Interrupt Clear register, or when the HPDMACR_DCP_VALID[3] bit of the descriptor 3 control register is set. |
| 12 | HPDMAEDR_DCP_NON_WORD_ERR[0] | 0 | Descriptor 0 non-word aligned transfer size error. 1: Descriptor 0 non-word aligned transfer size error 0: No non-word aligned transfer size error This bit is asserted High, if non-word aligned value is configured in descriptor 0 transfer size field. This bit is cleared on writing ‘1’ to HPDMAICR_NON_WORD_INT[0] of the HPDMA Interrupt Clear register, or when the HPDMACR_DCP_VALID[0] bit of the descriptor 0 Control register is set or when the HPDMACR_DCP_CLR[0] bit of the HPDMA Controller register is set. In this case, HPDMA will continue the transfer by ignoring the 2 LSBs of the transfer size field. |
| 13 | HPDMAEDR_DCP_NON_WORD_ERR[1] | 0 | Descriptor 1 non-word aligned transfer size error. 1: Descriptor 1 non-word aligned transfer size error 0: No non-word aligned transfer size error This bit is asserted High if a non-word aligned value is configured in the descriptor 1 transfer size field. This bit is cleared on writing ‘1’ to HPDMAICR_NON_WORD_INT[1] of the HPDMA Interrupt Clear register, or when the HPDMACR_DCP_VALID[1] bit of the descriptor 1 Control register is set, or when the HPDMACR_DCP_CLR[1] bit of the HPDMA Controller register is set. In this case, HPDMA will continue the transfer by ignoring the 2 LSBs of the transfer size filed. |
| 14 | HPDMAEDR_DCP_NON_WORD_ERR[2] | 0 | Descriptor 2 non-word aligned transfer size error. 1: Descriptor 2 non-word aligned transfer size error 0: No non-word aligned transfer size error This bit is asserted High if a non-word aligned value is configured in the descriptor 2 transfer size field. This bit is cleared on writing ‘1’ to HPDMAICR_NON_WORD_INT[2] of the HPDMA Interrupt Clear register, or when the HPDMACR_DCP_VALID[2] bit of the descriptor 2 Control register is set, or when the HPDMACR_DCP_CLR[2] bit of the HPDMA Controller register is set. In this case, HPDMA will continue the transfer by ignoring the 2 LSBs of the transfer size field. |
| 15 | HPDMAEDR_DCP_NON_WORD_ERR[3] | 0 | Descriptor 3 non-word aligned transfer size error. 1: Descriptor 3 non-word aligned transfer size error 0: No non-word aligned transfer size error This bit is asserted High, if a non-word aligned value is configured in the descriptor 3 transfer size field. This bit clears on writing ‘1’ to HPDMAICR_NON_WORD_INT[3] of the HPDMA Interrupt Clear register, or when the HPDMACR_DCP_VALID[3] bit of the descriptor 3 Control register is set, or when the HPDMACR_DCP_CLR[3] bit of the HPDMA Controller register is set. In this case, HPDMA will continue the transfer by ignoring the 2 LSBs of transfer size field. |
| [31:16] | Reserved | 0 | Software should not rely on the value of a reserved bit. To provide compatibility with future products, the value of a reserved bit should be preserved across a read-modify-write operation. |