5.34.119.1 Arguments
-timing_driven|-standard
Sets layout mode to be timing driven or standard (non-timing driven). The default is -timing_driven or the mode used in the previous layout command.
-place_incremental value
The following table shows the acceptable values for this argument:
Value | Description |
off | Discards previous placement. This is the default. |
on | Sets the previous placement as the initial starting point |
fix | Sets the previously placed macros’ locations as “FIXED” and continues to place the remaining ones |
-route_incremental value
The following table shows the acceptable values for this argument:
Value | Description |
off | Skips incremental mode, discards previous information. This is the default. |
Value | Description |
on | Invokes incremental mode, and sets the previous routing information as the initial starting point |
-run_placer value
The following table shows the acceptable values for this argument:
Value | Description |
on | Invokes placement. This is the default. |
off | Skips placement |
-run_router|-router|-route value
The following table shows the acceptable values for this argument:
Value | Description |
on | Invokes routing if placement is successful. This is the default. |
off | Skips routing |