5.34.122.1 Arguments
-timing_driven|-standard
Sets layout mode to be timing driven or standard (non-timing driven). The default is -timing_driven or the mode used in the previous layout command.
-place_incremental value
The following table shows the acceptable values for this argument:
Value | Description |
off | Discards previous placement. This is the default. |
on | Sets the previous placement as the initial starting point |
fix | Sets the previously placed macros’ locations as "fixed" and continues to place the remaining ones |