5.34.122.3 Arguments
-extended_run value
The following table shows the acceptable values for this argument:
Value | Description |
off | Skips extended run mode. This is the default. |
Value | Description |
on | Invokes extended run mode |
-placer_seed value
An integer value that you can set to change the initial random seed number for the placement.
-show_placer_seed
Causes Layout to display the initial random seed number used for the placement.