21.13.1.3 check_flash_memory
(Ask a Question)Description
The command performs diagnostics of the page status and data information as follows: • Page Status – includes ECC2 check of the page status information, write count • Page Data - ECC2 check
check_flash_memory [-name { device_name }] \
[-startpage { integer_value }] \
[-endpage { integer_value }] \
[-access { all | status | data }] \
[-show { summary | pages }] \
[-file { filename }]Arguments
| Parameter | Type | Description |
|---|---|---|
name | string | Optional user-defined device name. The device name is not required if there is only one device in the current configuration, or a device has already been selected using the set_debug_device command. |
startpage | integer | Startpage value must be an integer. You must specify a –endpage along with this argument. |
endpage | integer | Endpage value must be an integer. You must specify a –startpage along with this argument. |
access | string | You must set -startpage and -endpage before use. Specifies what NVM information to check: page status, data or both. All: Shows the number of pages with corruption status, data corruption and out-of-range write count (default). Status: Shows the number of pages with corruption status and the number of pages with out-of-range write count. Data: Shows only the number of pages with data corruption. |
show | string | This is an optional argument. You must set -startpage and -endpage before use. Specifies output level, as explained in the table below. Summary: Displays the summary for all checked pages (default). Pages: Displays the check results for each checked page. |
file | string | This is an optional argument. You must set -startpage and -endpage before use. Specifies name of output file for memory check. |
| Return Type | Description |
|---|---|
| None | None |
Error Codes
| Error Code | Description |
|---|---|
None | Parameter 'show' has illegal value. |
None | Parameter 'file' has illegal value. |
None | Parameter 'endpage' has illegal value. |
None | Missing '-endpage' argument for page range. Specify a page range with both a -startpage and an -endpage argument. |
None | Parameter 'startpage' has illegal value. |
None | Missing '-startpage' argument for page range. Specify a page range with both a -startpage and an -endpage argument. |
None | Parameter 'param_name' is not defined. Valid command formatting is'check_flash_memory [-deviceName "device name"] [-block "integer value"] [-client "client name"] [-startpage "integer value"] [-endpage "integer value"] [-access "all | status | data"] [-show "summary | pages"] [-file "filename"]'. |
None | Invalid value for -show: 'show_value'. Value should be 'summary' or 'pages'. |
None | endpage: Invalid argument value: 'endpage_value' (expecting integer value). |
None | startpage: Invalid argument value: 'startpage_value' (expecting integer value). |
None | Invalid value for -access: 'access_value'. Value should be 'all' or 'status' or 'data'. |
None | Missing specification for Flash Memory area. Use one of:-client [-block ]or-startpage -endpage -block. |
Supported Families
| SmartFusion 2 |
| IGLOO 2* |
| RTG4* |
Example
This example checks flash memory form pages 0 to 1 and saves their pages to check_flash_memory.txt file:
check_flash_memory -startpage 0 -endpage 1 \
-file {check_flash_memory.txt} \
-show {pages}See Also
read_flash_memory