21.13.1.78 write_active_probe
(Ask a Question)Description
This Tcl command sets the target probe point on the device to the specified value. The target probe point name must be specified.
write_active_probe [-deviceName device_name ] \
-name probe_name \
-value true|false \
-group_name group_bus_name \
-group_value "hex-value" | "binary-value"Arguments
| Parameter | Type | Description |
|---|---|---|
deviceName | string | Parameter is optional if only one device is available in the current configuration. |
name | string | Specifies the name for the target probe point. Cannot be a search pattern. |
value | boolean | Specifies values to be written. True = High, False = Low. |
group_name | string | Specify the group or bus name to write to complete group or bus. |
group_value | string | Specify the value for the complete group or bus. Hex-value format : "<size>'h<value>" Binary-value format: "<size>'b<value>" |
| Return Type | Description |
|---|---|
| None | None |
Error Codes
| Error Code | Description |
|---|---|
None | Parameter 'group_value' has illegal value. |
None | Active probe value must be specified. |
None | Parameter 'group_name' has illegal value. |
None | Parameter 'value' has illegal value. |
None | Parameter 'name' has illegal value. |
None | Parameter 'param_name' is not defined. Valid command formatting is'write_active_probe [-deviceName "device name"] \[-name "Probe point name"]* \[-value "TRUE | FALSE"]* \[-group_name "Group or Bus Name"]* \[-group_value "Group or Bus value"]* \[-silent "TRUE | FALSE"]'. |
Supported Families
| PolarFire |
| PolarFire SoC |
| SmartFusion 2 |
| IGLOO 2 |
| RTG4 |
Example
This example writes to a single probe.
write_active_probe –name out[5]:out[5]:Q –value trueThis example writes to a probe in the group:
write_active_probe -name grp1.out[3]:out[3]:Q -value "low"This example writes the value to complete group:
write_active_probe -group_name grp1 –group_value “8’hF0”This example writes multiple probes at the same time:
write_active_probe -group_name out \
-group_value “8’b11110000” \
-name out[2]:out[2]:Q \
-value trueSee Also
select_active_probe
read_active_probe
save_active_probe_list
load_active_probe_list