21.13.1.71 smartbert_test
(Ask a Question)Description
This Tcl command is used for the following:
Start a Smart BERT test - Start a test with a specified PRBS patterns on a specified SmartBERT lane.
Stop a Smart BERT test - Stop SmartBERT/PRBS test on a specified lane.
Reset error count - Reset counter of a lane during selected pattern test.
Inject error - Inject error into a SmartBERT IP lane.
smartbert_test -start -pattern {pattern name} \
-lane {Physical Location} \
[-smartbert_ip {TRUE | FALSE}] \
[-EQ-NearEndLoopback]
smartbert_test -reset_counter -lane {Physical Location}
smartbert_test -lane {Physical Location} [-inject_error {TRUE | FALSE}]
smartbert_test -stop -lane {Physical Location}Arguments
| Parameter | Type | Description |
|---|---|---|
deviceName | string | Optional user-defined device name. The device name is not required if there is only one device in the current configuration, or a device has already been selected using the set_debug_device command. |
lane | string | Specify the physical location of the lane. |
start | none | Start the Smart BERT test. |
pattern | string | Specify the pattern type of the Smart BERT test. Valid values of pattern type are: PRBS7, PRBS9, PRBS15, PRBS23 and PRBS31. |
smartbert_ip | boolean | This parameter applicable to the lane configured through SmartBERT IP. |
EQ-NearEndLoopback | none | Enable EQ-Near End Loopback on specified lane. |
reset_counter | none | Reset lane error counter on hardware and cumulative error count on the UI. |
inject_error | boolean | Specifies to inject error into a SmartBERT IP. Valid values are: TRUE or FALSE. |
stop | none | Stop the smart BERT test. |
| Return Type | Description |
|---|---|
| None | None |
Error Codes
| Error Code | Description |
|---|---|
None | SmartBert test: Must specify one of '-start', '-stop', '-reset_counter' or '-read_counter' arguments. |
None | SmartBert test: Lane Name not found in the list of assigned physical lanes in Libero. Provide the correct lane name. |
None | PRBS test: Invalid pattern type specified. |
None | SmartBert test: Is not a G5 Device. |
None | Parameter 'param_name' is not defined. Valid command formatting is 'smartbert_test [-deviceName "device name"] [-smartbert_ip "TRUE | FALSE"] [-start "TRUE | FALSE"] [-stop "TRUE | FALSE"] [-reset_counter "TRUE | FALSE"] [-read_counter "TRUE | FALSE"] [-pattern "Pattern type"] [-lane "Physical Lane Name"] [-EQ-NearEndLoopback "TRUE | FALSE"] [-inject_error "TRUE | FALSE"] '. |
Supported Families
| PolarFire |
PolarFire SoC |
Example
The following example starts Smart BERT test with a "prbs7" PRBS patterns on a "Q0_LANE0" SmartBERT lane:
# Transceiver lane without SmartBert IP without EQ-NearEndLoopback
smartbert_test -start -pattern {prbs7} -lane {Q0_LANE0}
# Transceiver SmartBERT IP lane
smartbert_test -start -smartbert_ip "TRUE" \
-pattern {prbs7} -lane {Q0_LANE0} \
-EQ-NearEndLoopback "TRUE"The following example resets counter of a "Q0_LANE0" lane during selected pattern test.
smartbert_test -reset_counter -lane {Q0_LANE0}The following stops Smart BERT/PRBS test on a "Q0_LANE0" SmartBERT lane:
smartbert_test -stop -lane {Q0_LANE0}The following example injects error into a "Q0_LANE0" SmartBERT IP lane:
smartbert_test -lane {Q0_LANE0} -inject_error {TRUE}See Also
prbs_test
loopback_mode
loopback_test