21.13.1.80 write_usram
(Ask a Question)Description
This tcl command writes a 12-bit word into the specified uSRAM location.
write_usram [-deviceName "device name"] \
[-name "USRAM block name"] \
[-logicalBlockName "USRAM user defined block name"] \
[-port "USRAM port name"] \
[-offset "integer value"] \
[-logicalValue "USRAM block word value"] \
[-value "integer value"]
Physical block
write_usram –name block_name \
–offset offset_value \
–value integer_value
Logical block
write_usram -logicalBlockName block_name \
-port port_name \
-offset offset_value \
-logicalValue hexadecimal_valueArguments
| Parameter | Type | Description |
|---|---|---|
deviceName | string | Optional user-defined device name. The device name is not required if there is only one device in the current configuration, or a device has already been selected using the set_debug_device command. |
name | string | Specifies the name for the target block. |
logicalBlockName | string | Specifies the name of the user defined memory block. |
port | string | Specifies the port of the memory block selected. Can be either Port A or Port B. |
offset | integer | Offset (address) of the target word within the memory block. |
logicalValue | integer | Specifies the hexadecimal value to be written to the memory block. Size of the value is equal to the width of the output port selected. |
value | integer | 12- bit value to be written. |
| Return Type | Description |
|---|---|
| None | None |
Error Codes
| Error Code | Description |
|---|---|
None | Parameter 'logicalValue' has illegal value. |
None | offset: Invalid argument value: 'offset_value' (expecting integer value). |
None | Parameter 'offset' has illegal value. |
None | Active probe value must be specified. |
None | Port_name is an invalid Port name. |
None | Parameter 'port' has illegal value. |
None | LSRAM port name must be specified. |
None | LSRAM block word cannot be written. Use phyical block word to write. |
None | Missing argument. Must specify '-name' or '-logicalBlockName'. |
None | Parameter 'value' has illegal value. |
None | Parameter 'name' has illegal value. |
Supported Families
| PolarFire |
| PolarFire SoC |
| SmartFusion 2 |
| IGLOO 2 |
| RTG4 |
Example
Writes a value of 0x291 to the device PolarFire in the Fabric_Logic_0/U3/F_0_F0_U1/ramtmp_ramtmp_0_0/INST_RAM64x12_IP with an offset of 0.
write_lsram \
-name {Fabric_Logic_0/U3/F_0_F0_U1/ramtmp_ramtmp_0_0/INST_RAM64x12_IP} \
-offset 0 \
-value 291write_usram -logicalBlockName {Fabric_Logic_0/U3/F_0_F0_U1} -port {Port A} -offset 1 -logicalValue {00FFF}See Also
read_usram