21.13.1.13 load_live_probe_list*
(Ask a Question)Description
This Tcl command loads the list of live probes from the file(*.txt).
load_live_probe_list [-deviceName "device name"] -file "filename"Arguments
| Parameter | Type | Description |
|---|---|---|
deviceName | string | Specify device name. This parameter is optional if only one device is available in the current configuration. |
file | string | Specify path and the name of input file(*.txt). This parameter is mandatory. |
| Return Type | Description |
|---|---|
| None | None |
Error Codes
| Error Code | Description |
|---|---|
None | Required parameter 'file' is missing. |
None | Parameter 'param_name' is not defined. Valid command formatting is 'load_live_probe_list [-deviceName "device name"] \ -file "filename"'. |
Supported Families
| PolarFire |
|
PolarFire SoC |
| SmartFusion 2 |
| IGLOO 2 |
| RTG4 |
Example
The following example loads M3T device live probes list from live_probe_list.txt file. Text file which has the probes list saved from previous SmartDebug save action.
save_live_probe_list -file {./live_probe_list.txt} load_live_probe_list
-deviceName {M3T} -file {./live_probe_list.txt}See Also
save_live_probe_list