21.13.1.39 plot_eye
(Ask a Question)Description
This Tcl command is used to plot eye and export eye plots.
plot_eye [-deviceName "device name"] \
-lane "Physical Lane Name" \
[-file "filename"]Arguments
| Parameter | Type | Description |
|---|---|---|
deviceName | string | Optional user-defined device name. The device name is not required if there is only one device in the current configuration, or a device has already been selected using the set_debug_device command. |
lane | string | Specify the lane instance name. |
file | string | Specify the path to the location where the file is to be exported. |
| Return Type | Description |
|---|---|
| None | None |
Error Codes
| Error Code | Description |
|---|---|
None | Required parameter 'lane' is missing. |
None | Parameter 'file' has illegal value. |
None | Plot Eye: Lane Name not found in the list of assigned physical lanes in Libero.Provide the correct lane name. |
None | Parameter 'lane' has illegal value. |
None | Parameter 'param_name' is not defined. Valid command formatting is 'plot_eye [-deviceName "device name"] -lane "Physical Lane Name" [-file "filename"] . |
Supported Families
| PolarFire |
| PolarFire SoC |
Example
This example plots eye for lane {Q2_LANE0} and saves it into {./export.txt} file.
plot_eye -lane {Q2_LANE0} -file {./export.txt}