21.13.1.51 read_flash_memory
(Ask a Question)Description
The command reads information from the NVM(Non volatile memory) modules. There are two types of information that can be read:
• Page Status – includes ECC1, ECC2, status, write count, access protection.
• Page Data
read_flash_memory [-deviceName { device_name }] \
[-startpage { integer_value }] \
[-endpage { integer_value }] \
[-access { all | status | data }] \
[-file { filename }]Arguments
| Parameter | Type | Description |
|---|---|---|
deviceName | string | Optional user-defined device name. The device name is not required if there is only one device in the current configuration, or a device has already been selected using the set_debug_device command. |
startpage | integer | Startpage is for page range. The value must be an integer. You must specify a -endpage and - block along with this argument. |
endpage | integer | Endpage is for page range. The value must be an integer. You must specify a -startpage and -block along with this argument. |
access | string | Specifies what eNVM information to check: page status, data or both. By default "all". |
file | string | Name of output file for memory read. |
| Return Type | Description |
|---|---|
| String | Displays page status and data of Flash Memnory Contet with plain text format. |
Error Codes
| Error Code | Description |
|---|---|
None | Parameter 'file' has illegal value. |
None | Parameter 'access' has illegal value. |
None | Parameter 'endpage' has illegal value. |
None | Parameter 'startpage' has illegal value. |
None | Parameter 'deviceName' has illegal value. |
None | Parameter 'param_name' is not defined. Valid command formatting is'read_flash_memory [-deviceName "device name"] [-block "integer value"] [-client "client name"] [-startpage "integer value"] [-endpage "integer value"] [-access "all | status | data | raw"] [-file "filename"]' |
Supported Families
| SmartFusion 2 |
| IGLOO 2* |
RTG4* |
Example
This example checks eNVM data information from 0 to 2 pages.
read_flash_memory -startpage 0 -endpage 2 -access {data} \
-file {flash_memory}See Also
check_flash_memory