21.13.1.72 static_pattern_transmit
(Ask a Question)Description
This Tcl command starts and stops a Static Pattern Transmit on selected lanes.
static_pattern_transmit -start -lane {Transceiver Physical Lane Name} \
-pattern {pattern_type} \
-value {user_pattern_value}
static_pattern_transmit -stop -lane {Transceiver Physical Lane Name} \
-pattern {empty} -value {empty}Arguments
| Parameter | Type | Description |
|---|---|---|
deviceName | string | Optional user-defined device name. The device name is not required if there is only one device in the current configuration, or a device has already been selected using the set_debug_device command. |
lane | string | Specify Transceiver physical Lane Name. |
start | none | Start the Static Pattern Transmit. |
stop | none | Stop the Static Pattern Transmit. |
pattern | string | Specify "pattern_type" of Static Pattern Transmit. "pattern_type" valid values are:
|
value | hexadecimal | Specify user_pattern_value in hex if pattern_type selected is custom. Takes the input pattern to transmit from the Lane Tx of selected lanes. Internal validators dynamically check the pattern and indicate when an incorrect pattern is given as input. |
| Return Type | Description |
|---|---|
| None | None |
Error Codes
| Error Code | Description |
|---|---|
None | Parameter 'param_name' is not defined. Valid command formatting is'static_pattern_transmit [-deviceName "device name"] [-start "TRUE | FALSE"] [-stop "TRUE | FALSE"] [-lane "Physical Lane Name"] [-pattern "Pattern type"] [-value "User pattern Value"]'. |
None | Static Pattern Transmit: Must specify one of '-start', '-stop' arguments. |
None | Static Pattern Transmit: Transceiver physical Lane Name must be specified. |
None | Static Pattern Transmit: Must specify pattern type argument. |
None | Static Pattern Transmit: Lane Name not found in the list of assigned physical lanes in Libero.Provide the correct lane name. |
None | Static Pattern Transmit: Invalid static pattern type specified. |
None | Static Pattern Transmit: Pattern Length exceeds the expected size. |
Supported Families
| PolarFire |
| PolarFire SoC |
Example
The following examples starts/stops fixed/maxrunlength Static Pattern transmit on "Q0_LANE0" /"Q0_LANE1" lane:
static_pattern_transmit -start -lane {Q0_LANE0} \
-pattern {fixed} -value {}
static_pattern_transmit -stop -lane {Q0_LANE0}
static_pattern_transmit -start -lane {Q0_LANE1}
-pattern {maxrunlength} -value {}
static_pattern_transmit -stop -lane {Q0_LANE1}The following examples starts/stops fcustom Static Pattern transmit on "Q2_LANE2" lane with "1010111" user pattern value:
static_pattern_transmit -start -lane {Q2_LANE2} \
-pattern {custom} -value {1010111}
static_pattern_transmit -stop -lane {Q2_LANE1}