21.13.1.49 read_snvm_memory
(Ask a Question)Description
This Tcl command reads client or page(s) in the sNVM (Secure Non volatile memory) memory from the device and returns a plain text (status and data of page).
If you have more than one client configured in Libero and use a client name with inappropriate -startpage, -endpage or -uskKey option values, then the command will fail.
read_snvm_memory [-deviceName "device name"] \
[-client "client name"] \
-startpage "integer value" \
-endpage "integer value" \
[-fileName "snvm data file name"] \
-uskKey "usk key"
Arguments
| Parameter | Type | Description |
|---|---|---|
deviceName | string | Optional user-defined device name. The device name is not required if there is only one device in the current configuration, or a device has already been selected using the set_debug_device command. |
client | string | Name of the client configured in Libero. |
startpage | integer | Start page number configured in Libero. |
endpage | integer | End page number. |
fileName | string | Name of output file for memory read. |
uskKey | hexadecimal | User Secret Key security key configured for the client in hexadecimal format |
| Return Type | Description |
|---|---|
String | Displays page status and data of sNVM memory with plain text format. |
Error Codes
| Error Code | Description |
|---|---|
None | Number of usk keys entered do not match with page range mentioned. |
None | The start page value is incorrect for the client entered. |
None | The end page value is incorrect for the client entered. |
None | Invalid usk key specified. Input should be either '0' or 24 hexadecimal characters. |
None | Parameter 'param_name' is not defined. Valid command formatting is 'read_snvm_memory [-deviceName "device name"] [-client "client name"] -startpage "integer value" -endpage "integer value" [-fileName "snvm data file name"] -uskKey "usk key"'. |
None | Parameter 'uskKey' has illegal value. |
None | Required parameter 'uskKey' is missing. |
None | Parameter 'fileName' has illegal value. |
None | Parameter 'endpage' has illegal value. |
None | Parameter 'startpage' has illegal value. |
None | Parameter 'client' has illegal value. |
None | Client name was not found. |
None | Parameter 'deviceName' has illegal value. |
None | Parameter 'startpage' must be a positive integer value. |
None | startpage: Invalid argument value: 'value' (expecting integer value). |
None | endpage: Invalid argument value: 'value' (expecting integer value). |
None | Parameter 'endpage' must be a positive integer value. |
Supported Families
| PolarFire |
PolarFire SoC |
Example
Read "0" startpages and "2" endpages from sNMV memeory from the device and save into svnm.txt file:
read_snvm_memory -startpage "0" -endpage "2" \
-fileName "snvm.txt" -uskKey {0:0:0}