21.13.1.23 load_active_probe_list
(Ask a Question)Description
This Tcl command loads the list of probes from the file.
load_active_probe_list [-deviceName "device name"] \
-file "path to the file"Arguments
| Parameter | Type | Description |
|---|---|---|
deviceName | string | Parameter is optional if only one device is available in the current configuration. |
file | string | The input file location. |
| Return Type | Description |
|---|---|
| None | None |
Error Codes
| Error Code | Description |
|---|---|
None | Parameter 'file' has illegal value. |
None | Required parameter 'file' is missing. |
None | Parameter 'param_name' is not defined. Valid command formatting is'load_active_probe_list [-deviceName "device name"] -file "filename"'. |
Supported Families
| PolarFire |
| PolarFire SoC |
| SmartFusion 2 |
| IGLOO 2 |
| RTG4 |
Example
This example loads the active probe list from “./my_probes.txt” file.
load_active_probe_list -file “./my_probes.txt”See Also
delete_active_probe
read_active_probe
save_active_probe_list
select_active_probe
write_active_probe