21.13.1.47 read_lsram
(Ask a Question)Description
This tcl command reads a specified block of large SRAM from the device.
read_lsram [-deviceName "device name"] \
[-name "LSRAM block name"] \
[-logicalBlockName "USRAM user defined block name"] \
[-port "LSRAM port name"] \
[-fileName "Data file name"] \
[-file "Data file name"]Arguments
| Parameter | Type | Description |
|---|---|---|
deviceName | string | Optional user-defined device name. The device name is not required if there is only one device in the current configuration, or a device has already been selected using the set_debug_device command. |
name | string | Specifies the name for the target block. |
logicalBlockName | string | Specifies the name for the user defined memory block. |
port | string | Specifies the port for the memory block selected. Can be either Port A or Port B. |
fileName | string | Optional; specifies the output file name for the data read from the device. |
file | string | Optional; specifies the output file name for the data read from the device. |
| Return Type | Description |
|---|---|
| None | None |
Error Codes
| Error Code | Description |
|---|---|
None | Parameter 'file' has illegal value. |
None | Parameter 'fileName' has illegal value. |
None | Port port_name is an invalid Port name. |
None | Parameter 'port' has illegal value. |
None | RAM port name must be specified. |
None | LSRAM block cannot be read. Use phyical block option to read. |
None | Parameter 'logicalBlockName' has illegal value. |
None | Missing argument. Must specify '-name' or '-logicalBlockName'. |
None | Parameter 'deviceName' has illegal value. |
None | Parameter 'param_name' is not defined. Valid command formatting is'read_lsram [-deviceName "device name"] [-name "LSRAM block name"] [-logicalBlockName "USRAM user defined block name"] [-port "LSRAM port name"] [-fileName "Data file name"] [-file "Data file name"]'. |
None | LSRAM block name failed to read: Target block not found in debug file. |
None | Parameter 'name' has illegal value. |
Supported Families
| PolarFire |
| PolarFire SoC |
| SmartFusion 2 |
| IGLOO 2 |
| RTG4 |
Example
Reads the LSRAM Block Fabric_Logic_0/U2/F_0_F0_U1/ramtmp_ramtmp_0_0/INST_RAM1K20_IP from the PolarFire device and writes it to the file output.txt.
read_lsram \
-name {Fabric_Logic_0/U2/F_0_F0_U1/ramtmp_ramtmp_0_0/INST_RAM1K20_IP} \
–fileName {output.txt}This example reads the uSRAM logical Block {Fabric_Logic_0/U3/F_0_F0_U1} from {Port A}.
read_lsram -logicalBlockName {Fabric_Logic_0/U2/F_0_F0_U1} -port {Port A}See Also
write_lsram