21.13.1.50 read_uprom_memory
(Ask a Question)Description
This Tcl command reads a uPROM memory block from the device.
If you have more than one clients configured in Libero and If you use client name with inappropriate -startaddress and -words then the command will fail.
read_uprom_memory [-deviceName "device name"] \
[-client "client name"] \
-startaddress "start address" \
-words "integer value" \
[-fileName "Data file name"]Arguments
| Parameter | Type | Description |
|---|---|---|
deviceName | string | Optional user-defined device name. The device name is not required if there is only one device in the current configuration, or a device has already been selected using the set_debug_device command. |
client | string | Specifie the name of client for memory read. Clients are configured in Libero tool under "device and memory initialisation". Those are a bunch of pages which can be used by the design to load data. Each client can have a different purpose. |
startaddress | hexadecimal | Specifies the start address of the uPROM memory block. |
words | integer | Specifies the number of 9-bit words. |
fileName | string | Name of output file for memory read. |
| Return Type | Description |
|---|---|
String | Displays page status and data of uPROM memory with plain text format.. |
Error Codes
| Error Code | Description |
|---|---|
None | Parameter 'deviceName' has illegal value. |
None | Parameter 'client' has illegal value. |
None | Parameter 'startaddress' has illegal value. |
None | Required parameter 'startaddress' is missing. |
None | Parameter 'words' has illegal value. |
None | Required parameter 'words' is missing. |
None | Parameter 'fileName' has illegal value. |
None | Invalid argument value: ' -word {1.0} ' (expecting integer value). |
None | Parameter 'param_name' is not defined. Valid command formatting is 'read_uprom_memory [-deviceName "device name"] [-client "client name"] -startaddress "start address" -words "integer value" [-fileName "Data file name"]'. |
None | The startaddress value is incorrect for the client entered. |
None | The word number is incorrect for the client entered. |
None | Parameter 'words' must be a positive integer value. |
Supported Families
| PolarFire |
PolarFire SoC |
Example
This example reads 10 9-bit words from uPROM memory '0xA' address :
read_uprom_memory –startaddress {0xA} –words {10}This example reads 9-bit words from uPROM memory '0xA' address :
read_uprom_memory -client {client1} \ -startaddress "2" \ -words "2" \ -fileName "./data.txt"