21.13.1.67 set_live_probe
(Ask a Question)Description
This Tcl command assigns channels A and/or B to the specified probe point(s). At least one probe point must be specified. Only exact probe name is allowed (that is, no search pattern that may return multiple points).
For RTG4, only one probe channel (Probe Read Data Pin) is available: A
set_live_probe [-deviceName "device_name" ] \
[–probeA "probe point A" ] \
[–probeB "probe point B" ]Arguments
| Parameter | Type | Description |
|---|---|---|
deviceName | string | Parameter is optional if only one device is available in the current configuration or set for debug. This parameter is optional. |
probeA | string | Specifies target probe point for the probe channel A. This parameter is optional. |
probeB | string | Specifies target probe point for the probe channel B. This parameter is optional. |
| Return Type | Description |
|---|---|
| None | None |
Error Codes
| Error Code | Description |
|---|---|
None | Parameter 'param_name' is not defined. Valid command formatting is 'set_live_probe [-deviceName "device name"] [-probeA "probe point A"] [-probeB "probe point B"] '. |
None | Parameter 'probeA' has illegal value. |
None | Cannot set live probes: Probe A is not found. |
None | Cannot set live probes: IDCode verify failed. |
Supported Families
| PolarFire |
|
PolarFire SoC |
| SmartFusion 2 |
| IGLOO 2 |
| RTG4 |
Exception
The array must be programmed and active.
Active probe read or write operation will affect current settings of Live probe since they use the same probe circuitry inside the device.
Setting only one Live probe channel affects the other one, so if both channels need to be set, they must be set from the same call to set_live_probe.
Security locks may disable this function.
To be available for Live probe, ProbeA and ProbeB I/Os must be reserved for Live probe respectively.
Example
The following example sets Live probe channel A to the probe point A12 on device sf2.
set_live_probe [-deviceName sf2] [–probeA A12]See Also
unset_live_probe