21.13.1.52 record_actions
(Ask a Question)Description
This sequence can be used to access registers from an external processor to perform the same actions done in SmartDebug, to provide the register sequence for each of the actions performed in the XCVR Debug Window.
Note:
This command is valid only when the XCVR block is presented in Libero Design.
record_actions -start_recording | -stop_recording -file {file name}Arguments
| Parameter | Type | Description |
|---|---|---|
deviceName | string | Optional user-defined device name. The device name is not required if there is only one device in the current configuration, or a device has already been selected using the set_debug_device command. |
start_recording | none | Specifies the moment of start recording. |
stop_recording | none | Specifies the moment of stop recording. |
file | string | Specify path and the name of output *.txt file. This parameter is mandatory when |
| Return Type | Description |
|---|---|
| None | None |
Error Codes
| Error Code | Description |
|---|---|
None | Parameter 'file' has illegal value. |
None | Start Record parameter already set. Recording is in progress. |
None | Record action parameters are absent. Either -start_recording or -stop_recording should ba passed as a parameter. |
None | Both parameters cannot be passed. Either -start_recording or -stop_recording should ba passed as a parameter. |
None | Error: Parameter 'param_name' is not defined. Valid command formatting is'record_actions [-deviceName "device name"] [-start_recording "TRUE | FALSE"] [-stop_recording "TRUE | FALSE"] [-file "file name"]'. |
Supported Families
| PolarFire |
PolarFire SoC |
Example
This example starts recording, then stops it and saves the recorded data in the {./actions} file.
record_actions -start_recording
record_actions -stop_recording -file {./actions.txt}