21.13.1.65 set_debug_programmer
(Ask a Question)Description
Identifies the programmer you want to use for debugging (if you have more than one).
set_debug_programmer -name { programmer_name }Arguments
| Parameter | Type | Description |
|---|---|---|
name | string | Specify the programmer. This argument is mandatory. |
| Return Type | Description |
|---|---|
| None | None |
Error Codes
| Error Code | Description |
|---|---|
None | Unable to select programmer 'prog_name' for debug. |
None | Required parameter 'name' is missing. |
None | Parameter 'param_name' is not defined. Valid command formatting is 'set_debug_programmer -name "programmer name"' |
None | Parameter 'name' has illegal value. |
Supported Families
| PolarFire |
| PolarFire SoC |
| SmartFusion 2 |
| IGLOO 2 |
| RTG4 |
Example
The following example selects the programmer 10841:
set_debug_programmer -name {10841}