21.13.1.41 process_job_request
(Ask a Question)Description
Processes a job request received from Job Manager. It is part of the Job Ticket generation process.
Note: The HSM server name must be specified using the HSM_SERVER_NAME DEF variable.
process_job_request -request_file "job request file" -reply_file "job reply file" [-overwrite_reply "TRUE | FALSE"]
Arguments
Parameter | Type | Description |
---|---|---|
request_file | string | Specifies the full file name of the job request file. This argument is mandatory. |
reply_file | string | Specifies the full job name of the job reply file. |
overwrite_reply | string | Optional parameter.
|
Error Codes
Error Code | Description |
---|---|
None | Required parameter "request_file" is missing. |
None | None Required parameter "reply_file" is missing. |
None | Parameter "request_file" : the file "/request_file_name" does not exist. |
None | overwrite_reply: Invalid argument value: "value" (expecting TRUE, 1, true, FALSE, 0 or false). |
None | Cannot get HSM. |
None | Parameter "param_name" is not defined. Valid command formatting is "process_job_request -request_file "job request file" \ -reply_file "job reply file" \ [-overwrite_reply "TRUE | FALSE"]". |
Supported Families
PolarFire |
SmartFusion 2 |
IGLOO 2 |
Example
This example processes a job request.
process_job_request \
-request_file {D:/flashpro_files/jobmgr_project/cm_request.req} \
-reply_file {D:/flashpro_files/jobmgr_project/cm_reply.rep} \
-overwrite_reply {TRUE}