13.4.3.12 SPI Command Register
The following table describes the Command register..
| Bit Number | Name | R/W | Reset Value | Description |
|---|---|---|---|---|
| [31:7] | Reserved | R/W | 0 | Software should not rely on the value of a reserved bit. To provide compatibility with future products, the value of a reserved bit should be preserved across a read-modify-write operation. |
| 6 | TXNOW | R/W | 0 | 0: No effect 1: Writing one clears the TxBUSY bit in slave mode immediately rather than waiting for PKTSIZE frames to be available, telling the master that there is data available. This is intended to use when less than the programmed PKTSIZE data frames are being transmitted, removing the requirement to transmit PKTSIZE frames. This bit stays set until the first data frame is transmitted. |
| 5 | AUTOSTALL | R/W | 0: No effect 1: Writing one will cause the master to delay transmission until the transmit FIFO contains the number of frames specified by the Table 13-22 register. This guarantee that the frames are transmitted with no idle cycles or time gaps between them. This bit will be automatically cleared as soon as the core starts transmitting the frames. | |
| 4 | CLRFRAMECNT | R/W | 0: No effect 1: Writing one clears the internal frame counter. This bit always reads as zero. The counter is also cleared when the core is disabled, CTL1, or CTL2 are written (that is, the frame count limit changed). | |
| 3 | TXFIFORST | R/W | 0 | 0: No effect 1: Writing one resets the Tx FIFO. This bit always reads as zero. |
| 2 | RXFIFORST | R/W | 0 | 0: No effect Writing one resets the Rx FIFO. This bit always reads as zero. |
| 1 | AUTOEMPTY | R/W | 0 | 0: No effect 1: Writing one causes the SPI core to automatically discard any further received data until the number of frames requested in the FRAMECNT register has been received or (in slave mode) SSEL goes inactive. This bit will stay set until all the frames are complete or it is cleared. |
| 0 | AUTOFILL | R/W | 0 | 0: No effect 1: Writing one causes the SPI core to automatically fill the transmit FIFO with zeros to match the number of frames requested in the FRAMECNT register. Typically, the five command bytes must be written to the TxDATA register and then this bit must be set. Data can be read from the receive FIFO until the complete set of frames has been read. This bit will stay set until all the frames are complete or it is cleared. |