2.90.37 PWM_GENERATOR Enum
Summary
Defines the PWM generators that are selected from the MCC Harmony User Interface for the PWM output controls.
Description
The "PWM_GENERATOR" enum represents the different PWM generators available for configuration through the MCC Harmony User Interface. These values correspond to specific hardware PWM generators that can be used for generating PWM outputs. The generated list in the help documentation may not represent all the channels but is based on the user's configuration in the MCC Harmony tool. The user should configure the PWM generators according to their application requirements. The generated enum list may vary depending on the specific PWM Generators are enabled in User Interface.
Remarks
None.