Description
This Tcl command changes the source of all the linked files in your project.
change_all_links -current_path {current source path} \
-new_path {new source path}
Arguments
Parameter | Type | Description |
---|
current_path | string | Current source path of linked files. It is mandatory. |
new_path | string | New source path of linked files. It is mandatory. |
Return Type | Description |
---|
None | None |
Error Codes
Error Code | Description |
---|
None | No files are linked in the project from the specified current path. Please check the path. |
None | Param 'new_path' should not be empty. |
None | Parameter 'new_path' has illegal value. |
None | Required parameter 'new_path' is missing. |
None | Parameter 'current_path' has illegal value. |
None | Required parameter 'new_path' is missing. |
None | Parameter 'param_name' is not defined. Valid command formatting is 'change_all_links -current_path "current_path" -new_path "new_path"'. |
Supported Families
Supported Families |
PolarFire® |
PolarFire SoC |
RTG4™ |
SmartFusion® 2 |
IGLOO® 2 |
Example
Change the source of all the link files in project from “./src/link_source_old” to “./src/link_source_new”
change_all_links -current_path {./src/link_source_old} \
-new_path {./src/link_source_new }