Description
This Tcl command removes a link to a file in your project and it is not removed link to a folder. You can unlink a file form a folder, and to unlink the whole folder you have to unlink all files one by one from the link folder.
unlink_files \
[-file {absolute or related path and name of the linked file}] \
[-from_disk {0|1}]
Arguments
Parameter | Type | Description |
---|
file | string | Absolute or relative path and name of the linked (remote) file you want to unlink. There may be multiple -file arguments (see example below). You can repeat this argument to unlink multiple files. |
from_disk | boolean | Removes file from disk. Valid values are: TRUE or 1, FALSE or 0. |
Error Codes
Error Code | Description |
---|
None | Parameter 'file' is missing or has invalid value. |
None | Required parameter 'file' is missing. |
None | Unable to find the file. |
None | Parameter 'param_name' is not defined. Valid command formatting is 'unlink_files [-file "file"]+ [-from_disk "TRUE | FALSE"] ' . |
Supported Families
Supported Families |
PolarFire® |
RTG4™ |
SmartFusion® 2 |
IGLOO® 2 |
Example
- Unlink the file file1.vhd from my project.
unlink_files -file {E:\Share\file1.vhd}
- Unlink files “E:\Share\abc.v” and “E:\Share\abc.sdc" from the project using Environment variable “MSCC_ROOT_1” that has the root directory path “E:\Share”.
unlink_files -file {${MSCC_ROOT_1}/abc.v} -file {${MSCC_ROOT_1}/abc.sdc}