Description
This Tcl command checks the HDL in the specified file for validity.
check_hdl -file { absolute path and name of the HDL file }
Arguments
Parameter | Type | Description |
---|
file | string | Specified absolute path and name of the HDL file you want to check. It is mandatory. |
Error Codes
Error Code | Description |
---|
None | HDL file is not in the project. |
None | Required parameter 'file' is missing. |
None | Parameter 'file' has illegal value. |
None | Parameter 'param_name' is not defined. Valid command formatting is 'check_hdl
-file "file"'. |
Supported Families
Supported Families |
PolarFire® |
RTG4™ |
SmartFusion® 2 |
IGLOO® 2 |
Example
The following command checks HDL on the file hdl1.vhd.
check_hdl -file {/project/hdl/hdl1.vhd}