21.3.63 one_way_passcode

Description

This Tcl command enables/disables One Way Passcode (OWP).

Important: This Tcl command is applicable for Libero SoC Design Suite v2022.3 and later.
one_way_passcode -enable true/false (or 0/1) 

Arguments

Parameter Type Description
enable boolean

Enter 1 to enable or 0 (default) to disable One-Way Passcode (OWP).

Enter true to enable or false (default) to disable One-Way Passcode (OWP).

Return Type Description
None None

Error Codes

Error Code Description
None NA

Supported Families

PolarFire® SoC

Example

The following example enables One Way Passcode (OWP).

one_way_passcode -enable 1
one_way_passcode -enable true