21.3.9 change_vault_location

Description

This Tcl command changes the location of the vault. Equivalent to clicking the Project menu, and choosing Vault/Repositories Setting and selecting new vault location, by default is "/usr/local/Microchip/common"/. The vault location is common to all Microchip software:
  • Project Manager
  • Firmware Catalog

Changing your vault location here updates the vault location for all the Microchip tools you use on your machine.

Important: This command overrides the vault location for all projects.
change_vault_location -location location

Arguments

Parameter Type Description
location string Specifies the new vault location. Value must be a file path. It is mandatory.
Return Type Description
None None

Error Codes

Error Code Description
None

Required parameter 'location' is missing.

None Parameter 'location' is missing.
None

Parameter 'param_name' is not defined. Valid command formatting is 'change_vault_location -location "location" ' .

Supported Families

Supported Families
PolarFire®
RTG4
SmartFusion® 2
IGLOO® 2

Example

The following command changes the old location of vault into new location.

change_vault_location -location {new_vault_path/vault}