Description
This Tcl command exports the IBIS (Input/Output Buffer Information Specification) model report. The IBIS model report provides an industry-standard file format for recording parameters like driver output impedance, rise/fall time, and input loading, which may then be used by software applications such as Signal Integrity tools or IBIS simulators. The exported file has a *.ibs(name <root>.ibs) file name extension.
export_ibis_file -file {absolute or relative path and name of *.ibs file}
Arguments
Parameter | Type | Description |
---|
file | string | Specifies the absolute or relative path and name of IBIS file to export. If the file path is not specified, the file is created in <project_name>/designer/<design_name> directory. |
Error Codes
Error Code | Description |
---|
None | Parameter 'file' has illegal value. |
None | Required parameter 'file' is missing. |
Supported Families
Supported Families |
PolarFire® |
RTG4™ |
SmartFusion® 2 |
IGLOO® 2 |
Example
The following command exports the IBIS (Input/Output Buffer Information Specification) model report.
export_ibis_file -file {E:/designs/export/sd1.ibs}