Description
This Tcl command is intended for unsetting a global include file.
unset_global_include_file -file {filename}
Arguments
Parameter | Type | Description |
---|
file | string | The user provides the file path to unset as global include file. |
Return Type | Description |
---|
None | None |
Error Codes
Error Code | Description |
---|
None | Invalid Global Include File 'value'. |
None | Parameter 'file' has illegal value. |
None | Required parameter 'file' is missing. |
None | Parameter 'param_name' is not defined. Valid command formatting is 'unset_global_include_file -file "unset global include file"'. |
Supported Families
Supported Families |
PolarFire® |
PolarFire SoC |
RTG4™ |
SmartFusion® 2 |
IGLOO® 2 |
Example
This example unsets {./src/define.h} global include file.
unset_global_include_file -file {./prj/hdl/define.h}